The absolute maximum rating for the analog inputs to the ADC at the low end is -0.3V. Recommended anlog input range is 0 to AVDD (+3.3V). With a 2Vpp input, wouldn't AC-coupling cause the input signal to swing to -1V, violating the spec?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
The absolute maximum rating for the analog inputs to the ADC at the low end is -0.3V. Recommended anlog input range is 0 to AVDD (+3.3V). With a 2Vpp input, wouldn't AC-coupling cause the input signal to swing to -1V, violating the spec?
Hi Ted,
The analog input voltage specs that you are referring to is for the analog input pins voltage to AVSS.
If you scroll down to 7.5 Electrical Characteristics, you'll read that the Full-scale AC-coupled input signal is actually 1 Vrms, which is about 2.8 Vpp. You can also be reassured by the typical application shown in section 9.2, where you will find 1uF AC-coupling capacitors on each audio input. Hope this helps!
Best,
Andrew
I still contend that table 7.1 is unclear regarding the Analog input voltage to AVSS (analog supply ground). An AC-coupled 1Vrms signal will go below -0.3V.