This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi Gianluca
24V is indeed one of the item that may cause large power dissipation. Please let us know what is the load resistance value? And what is the output power for each channel? The PWM frequency, we chosen 768KHz or others? And the modulation mode, we chosen BD, or 1SPW, or Hybrid?
Hi Gianluca
The device is 50 watts per channel @ 24v.
The speakers are 4 ohm - 30 watts.
I'm a little confused about the power you are using. The speaker is 30W but the device output 50W? Seems not reasonable.
Anyway, below is some test results at our side, for your reference.
We tested the EVM under 24V, 1SPW, 768KHz, 3ohm load, and output 2*42W for more than half an hour, the device still not OT shutdown. But the temperature would be very high, around 100C at the heatsink, and the device Die temperature really close to 160C. Heatsink is 78mm*36mm*36mm on the EVM.
So for your condition, the heatsink is still seems not large enough.