Hello guys,
I want to implement a SW function, that the TAS5782M can be used either in Mono or Stereo mode.
For me, the information in the datasheet is ambiguous.
Here, it shows that SPK_INB+ and SPK_INB- are supposed to be grounded. Additionally, the post implies that this is a requirement to mono mode.
e2e.ti.com/.../tas5782m-asking-for-the-tas5782-mono-application
However, the datasheet doesn't state this. Moreover, it says that a mixture of two channels can be used in mono mode. If I for example set the input mixer to route 100% left audio input data to both output stages and 0% of the right audio input, I can create a mono signal as well.
Hence the question: Do I need to connect SPK_INB+ and SPK_INB- to GND in Mono mode or can I set the TAS5782M to mono mode purely in software?
Thanks and regard,
Stefan