Dear Sir,
We have a similar problem.
I am confused on how to configure this chipset.
We need ro configure the cipset to work with 48khz, 16bit mono pcm mode only.
Hence when i calculate the bclk it should equal to 48×16bit =758KHZ.
However there is no option of such a clock speed on the ppc3 integration app. The only option is 1.536 MHZ or higher.
Furthermore is it correct to say because the bclk is lower than 1 mhz , then it is needed to use mclk.
We tried to use the ppc3 config registers , however we can hear sound it seems completly garbled.
I am also curious to know what it means by meta burst? Is there a special way to send i2c commands in burt mode..
Thanking you
Nadeem