Hi team,
If I disable DC OFFSET detect feature by setting DC_DET_CTRL Register(0x6) bit 0 (DC_DETECT_DIS,
then DC offset fault will no more be reported on OC DC FAULT Mem register (0x8E)?
1. I don't want to disable Output at least xx seconds after I detect DC offset detection.
2. I would like to detect DC offset fault and manually disable the output.
Is that possible to control DC offset fault as such?
regards,