This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TAS5760M: About power consumption.

Part Number: TAS5760M

Hi team

I have a question about power consumption.

The conditions of use are as follows.

【conditions】
 PVDD: 24V
 Rspk: 8Ω
 SPEAKER AMPLIFIER STATE: fspk_AMP =768kHz,Shutdown

【question】
①The following values listed in the data sheet are TYP values, right?

 IPVDD+AVDD: 0.078mA
 IDVDD:0.03mA

②Please tell me the value of MAX and MIN.

③When DVDD is 0V, does IDVDD also become 0mA?


Best Regards
S.Miura