This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPA3139D2: Spec question

Part Number: TPA3139D2

Hi,

I have several question about TPA3139D2 Class D Amplifier.

1) In datasheet chapter 6.1 absolute Maximum Ratings. Minimum load Resistor is 4.8 ohm @ BTL, (10V < PVCC <14.4V) condition.

But 4 ohm speaker application is record in this datasheet figure 6-5 output power vs supply voltage 

Can I use 4 ohm speaker in AVCC=PVCC=12V condition?

2) I need more detail ferrite bead selection guide to design my board to comply FCC class B EMI regulation.

In datasheet page 25, It only recommend to use Murata NFZ2MSM series ferrite bead.

But I don't know the requirement to select proper ferrite bead.

Regards,

Harry Wang

2023/09/01