This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DRV601: DRV600/DRV601 Line Driver

Part Number: DRV601
Other Parts Discussed in Thread: DRV600, , DRV134, DRV135

Hi TI members,

I have to drive 150Ω audio load impedance with a line driver. The  DRV600/DRV601 can be drive minimum load impedance of 100Ω, but I need to a differential input and a differential output line driver. The DRV601 does't support differential line input and line output.

I need to your suggest IC or something else.

NOTE: The Audio CODEC output load impedance is minimum 600Ω to 10kΩ.