Part Number: SRC4190-Q1
Can the device be used with word lengths less than 16 bit (down to 8)? Ik want to use the device in I2S mode with a number of different word lengths and sample rates.
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: SRC4190-Q1
Can the device be used with word lengths less than 16 bit (down to 8)? Ik want to use the device in I2S mode with a number of different word lengths and sample rates.
Hi Bert,
According to DS, The audio data word length may be up to 24 bits for I 2S and left justified formats, while the right justified format supports 16-, 18-, 20-, or 24-bit data.
Refer to table 2 ( Input Port Data Format Selection) to set it to I2S format.
Regards,
Arash