When using the PCM1820 in I2S Slave mode, how long do I have to wait between applying the clock signals (FSYNC and BCLK) and receiving valid samples on SDOUT?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
When using the PCM1820 in I2S Slave mode, how long do I have to wait between applying the clock signals (FSYNC and BCLK) and receiving valid samples on SDOUT?
This should be dependent on the decimation filter choosen. The group delay specification should give you the delay in FSYNC's
Given that the decimation filter is likely to be symmetrical, it should take twice the group delay for the filter to fully settle. And that doesn't allow the chip any time to detect the FSYNC frequency, to determine which decimation filter to apply.
Tha application of FSYNC and BCLK shall trigger the Automatic Clock Detection. This is based on counting to number of BCLKs in one FSYNC.This should take a minimum time of 1FSYNC to count BCLKS.
After this the Internal Clock setup and selection of decimation filter happens.