Hello,
I'm considering to load the configuration of TAS5825M from a connected SPI EEPROM. Unfortunately, after reading slaa847 there are still some questions left for me:
1. How is a load of the configuration initiated/started? Is there a special command or does it just happen after pulling CS low as suggested in slaa847 (3.3. - 6.)?
2. How does the TAS5825M know that the end of the configuration file is reached?
3. I would like to put multiple configuration files into one EEPROM and start loading from different starting addresses - is this possible?
4. Is it OK to pull CS high after successful loading?
5. Is there a preferred part or is any SPI EEPROM suited? Are there timing requirements available for the SPI port?
Best Regards.