This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPA3136D2: Regarding to the LC filter

Part Number: TPA3136D2

Hello team,

I received a question from the customer.

When the LC filter constant is configured with 10uH and 2.2uF, no audio is output. Could you please investigate the cause?

The conditions are as follows.

[1] Based on the evaluation results of EMI measurement, an LC filter was implemented in the audio output section of the TPA3136D2 as an emission countermeasure.

[2] The filter is configured with the recommended constants of 33uH and 1uF in the data sheet for a speaker impedance of 8Ω.

[3] Confirmation of normal operation

[4] Changed the constants in consideration of the mounting conditions, and changed the configuration to 10uH, 2.2uF, which is close to the constants and cutoff frequency on the data sheet.

[5] Output voltage became 6V constant for both positive and negative, and no sound was output.

Regards,

Masa