Hi,
Could we provide the chart of THD+N vs output power at VCC=12V and RL= 4Ohm application?
Target output tis 15W and want to check its THD+N performance.

Thanks and Best regards,
Tiger
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi,
Could we provide the chart of THD+N vs output power at VCC=12V and RL= 4Ohm application?
Target output tis 15W and want to check its THD+N performance.

Thanks and Best regards,
Tiger
Hi Tiger,
The chat Figure 12 in datasheet is at 12V VCC and load is 4ohm.
15W THD is almost 10%. If you want to check more detail performance, you can apply one EVM board and test.
Regards
Derek
Thanks Derek.
It looks BTL is a little limitation for these condition. Thus, do BU have the chart for VCC=12V and RL= 4Ohm in PBTL application?
Best regards,
Tiger
Hi Tiger
For this using condition, the BTL is not the limitation, the VCC12V voltage is the limitation.
In the datasheet, Rdson value of this device is 240mohm, and usually output inductor have another 50mohm Rdc. There's two Rdson and two inductor to divide the voltage with your 4ohm load. When only 12V voltage supply, only 10.4V voltage Max could give to load. And using this value as sinewave peak, you even can't get 15W output. So the output will already clipping when working to that power, that's why you would see THD quickly going up in the chart.
Changing to PBTL won't able to have any difference, the voltage is not large enough to create larger current, or power.
Hi Shadow,
However, it should be okay to 15W with 1% THD+N at 4Ohm speaker and 12V according to Figure 32 for PBTL.
But it should be a risk to have 15W 1% THD+N with 12V for sure.
Thus, will recommend to using higher PVCC.


Thanks and Best regards,
Tiger