This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LM4889: Reflow profile.

Guru 10800 points
Part Number: LM4889

Hi team,

My customer wants to change the reflow profile.
They are considering a peak temperature of 225°C within 50 seconds(MIN 15 sec) after sufficient preheating.
But, TI's recommended condition is 260°C peak.
If the peak temperature is lower, is there any concern below?
 *IC reliability
 *Mounting

BR,
Kengo.