Hi,
I am trying to drive the TAS5705EVM2 with an external I2S source. The SCLK, LRCLK and SDIN1 is connected using shielded cable to the jumper located on the PSIA, the MCLK is remain the same using the onboard signal soucre.The distance between my test circuit to EVM is approximately right next to each others.
My I2S source sampling rate is 48KHz and 16bits and the GUI setting is the same.
Problem:
The output sound is continuous but cracking, I just about hear the tone but not the word.
Question:
1, Do I need to modify the circuit in order to make it works?
2, Are there any options exist in the GUI that I could try?
Any suggestion I would be appreciated
many thx
sk