Part Number: TAS5828M
Other Parts Discussed in Thread: TAS3251
Hello everybody,
does anyone have any suggestions about which speaker to use in combination with the TAS5828M amplifier?
First of all, the amp is set in BTL mode, 1SPW modulation, and powered by a stable 24v.
I'm wondering which of these two speakers best fit the amp:
1) 30W RMS, 4 ohm, 87.5 dB sensitivity. Reference: Dayton Audio RS100-4
2) 40W RMS, 8 ohm, 89.4 dB sensitivity. Reference: Markaudio CHR-90
I'd like to use the second speaker, but I'm a little bit worried about the overall volume output considering it's a 8ohm speaker, regardless of the slightly high sensitivity.
The amp documentation is a little bit confusing for me about output performance for 8 ohm loads, nor have I the required knowledge to have a clearer idea about that.
Any suggestion or technical consideration about the amp will be highly appreciated.
Thanks.