Hi,
I am attempting to use the TLV320ADC6140 to record high frequency signals in a physics experiment.
My target sampling rate is 384 kHz 32-bit recording on 2 channels, but the best I have been able to accomplish is 192 kHz on 2 channels. I set this in the Line Properties settings in Windows 10. The format options I have go no higher than 192 kHz.
I am using the TLV320ADC6140 with the AC-MB and I am using the USB interface for communication. I have installed the PurePath Console and the TI UAC instrument drivers.
Is it possible to configure the TLV320ADC6140-EVM for 384 kHz sampling rates with it operating in slave mode and operating over the USB interface?