Hi,
I am using a 3 wire I2S configuration with the PCM5142. It is in I2C mode. Master device for the I2S and I2C is a QCC5125 (BTM525). I made a PCB for the PCM5142 according to the schematic below and there is no audio. VNEG is at 0.5V instead of -3.3V. DVDD, CPVDD, and AVDD are at 3.3V. LDO is 1.9V. The issue is not with the source (QCC5125). I checked the clock outputs and the I2C bus of the master source and they are working fine. DOUT is also outputting data to the DIN of the PCM5142. Any help is appreciated.
Schematic:
PPS:
WCLK clock:
BCLK clock:
PPS code: