Other Parts Discussed in Thread: TAS5634
Hi
I want to use TPA3255 amplifier board with 13S battery. With full charge battery will reach to 54.6V. Can you tell me, if that can work. you say 53.5V on 6ohm. i will using 4ohm driver. but TPA3255 also say max V is 69 (or 63V). So therefore i'm wonder if i can use 54.6V battery? the bigger caps on the board i can see are 63V.
Thank you very much