Part Number: TLV320ADC3140
Hi team,
In slave mode with 4 channels of single-ended analog inputs, the only way to send data to the master device via standard I2S is to set GPIO1 to SDOUT2.
In this case, there is no external MCLK input port, so a PLL may be used.
I would like to know what register settings are necessary in this case.
I am planning to input the clock as follows
FYNC = sampling frequency Fs = 12.8kHz or 25.6kHz or 51.2kHz
BCLK = 64 x Fs input
In addition, FS_RATE[3:0] in MST_CFG1 Register (page = 0x00, address = 0x14) [reset = 48h] should be set to "Programmed sample rate of the ASI bus (not used when the device is configured in slave mode auto clock configuration). This is the auto clock configuration.
Does this mean that it can be used in slave mode without auto clock configuration?
Sincerely,
Ryu.