This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TLV320AIC3106: Power consumption assessment

Part Number: TLV320AIC3106

Hi Team,

My customer wanted to evaluate the power consumption of the AIC3106, but the specification gave multiple reference standards.

Can you help confirm which standard customers should refer to? And how do I determine the status of the device

The following is the customer's current software configuration.

page       reg  val (16进制)   val (10进制)

0      0      0x00        0

0      1      0x00        0

0      2      0x00        0

0      3      0x10        16

0      4      0x04        4

0      5      0x00        0

0      6      0x00        0

0      7      0x00        0

0      8      0x00        0

0      9      0x00        0

0      10    0x00        0

0      11    0x01        1

0      12    0x10        16

0      13    0x00        0

0      14    0x00        0

0      15    0x04        4

0      16    0x80        128

0      17    0xFF 255

0      18    0xFF 255

0      19    0x78        120

0      20    0x78        120

0      21    0x80        128

0      22    0x78        120

0      23    0x78        120

0      24    0x78        120

0      25    0x06        6

0      26    0x00        0

0      27    0xFE 254

0      28    0x00        0

0      29    0x00        0

0      30    0xFE 254

0      31    0x00        0

0      32    0x00        0

0      33    0x04        4

0      34    0x00        0

0      35    0x00        0

0      36    0x80        128

0      37    0x00        0

0      38    0x00        0

0      39    0x00        0

0      40    0x00        0

0      41    0x00        0

0      42    0x00        0

0      43    0x80        128

0      44    0x80        128

0      45    0x00        0

0      46    0x00        0

0      47    0x00        0

0      48    0x00        0

0      49    0x00        0

0      50    0x00        0

0      51    0x04        4

0      52    0x00        0

0      53    0x00        0

0      54    0x00        0

0      55    0x00        0

0      56    0x00        0

0      57    0x00        0

0      58    0x04        4

0      59    0x00        0

0      60    0x00        0

0      61    0x00        0

0      62    0x00        0

0      63    0x00        0

0      64    0x00        0

0      65    0x04        4

0      66    0x00        0

0      67    0x00        0

0      68    0x00        0

0      69    0x00        0

0      70    0x00        0

0      71    0x00        0

0      72    0x04        4

0      73    0x00        0

0      74    0x00        0

0      75    0x00        0

0      76    0x00        0

0      77    0x00        0

0      78    0x00        0

0      79    0x00        0

0      80    0x00        0

0      81    0x00        0

0      82    0x00        0

0      83    0x00        0

0      84    0x00        0

0      85    0x00        0

0      86    0x00        0

0      87    0x00        0

0      88    0x00        0

0      89    0x00        0

0      90    0x00        0

0      91    0x00        0

0      92    0x00        0

0      93    0x00        0

0      94    0x00        0

0      95    0x00        0

0      96    0x00        0

0      97    0x00        0

0      98    0x90        144

0      99    0x40        64

0      100  0x00        0

0      101  0x00        0

0      102  0x02        2

0      103  0x00        0

0      104  0x00        0

0      105  0x00        0

0      106  0x00        0

0      107  0x00        0

0      108  0x00        0

0      109  0x00        0

0      110  0x00        0

0      111  0x00        0

0      112  0x00        0

0      113  0x00        0

0      114  0x00        0

0      115  0x00        0

0      116  0x00        0

0      117  0x00        0

0      118  0x00        0

0      119  0x00        0

0      120  0x00        0

0      121  0x00        0

0      122  0x00        0

0      123  0x00        0

0      124  0x00        0

0      125  0x00        0

0      126  0x00        0

0      127  0x00        0

BR

Adrian