Part Number: PCM1861-Q1
Other Parts Discussed in Thread: PCM1681-Q1,
Hi team,
Can PCM1681-Q1 support 6CH TDM? Could you help to provide the related description in datasheet?
BRs,
Haury
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: PCM1861-Q1
Other Parts Discussed in Thread: PCM1681-Q1,
Hi team,
Can PCM1681-Q1 support 6CH TDM? Could you help to provide the related description in datasheet?
BRs,
Haury
Hi Harry,
Your ticket has two part numbers listed. Can you clarify if you're talking about the PCM1861-Q1 or PCM1681-Q1?
Thanks,
Jeff McPherson
Hi Harry,
In section 8.3.4 of the datasheet, it says that the device supports TDM8, and is only supported in the multiples 128, 256, and 512fs. TDM8 is much more typical and friendlier to the clock set up. TDM6 would be possible only if the clocking was setup for TDM8 and the last two channels are blank.
Best regards,
Jeff McPherson