Hi, Support Team
We saw the datasheet 6.3.7.1.6 have some question
6.3.7.1.6 Input Pin Short to VBAT_IN
A short to VBAT_IN fault occurs when the difference between the voltage measured for the VBAT_IN pin and the
input pin, ABS(VBAT_IN – INxx), is less than the threshold or both the VBAT_IN and INxx pin measured voltages
are above 11.7V. The threshold can be set by configuring DIAG_SHT_VBAT_IN, P1_R71_D[3:0].
When VBAT_IN is less than MICBIAS, false fault detections can exist based on the signal level of the INxx
pin. To minimize false detections there is also a separate debounce count for this condition set by configuring
VSHORT_DBNCE, P1_R74_D1.
---------------------------------------------------------------------------------------------------------------------------------------------------------
if VBAT_IN voltage is setting 8V and MICBIAS also is 8V, The Codec could possible easy occurs fail?
have any side effect
if any suggestion, Please advise me.
Thanks,
Best regards,
Lawrence