Other Parts Discussed in Thread: TAC5111
Hi,
I'm working on verifying a custom board with TLV320AIC1110, but the loopback function isn't working as expected.
So, could you please tell me the following?
Q1
Is it correct to understand that the PCM loopback set by the 5th bit of the Mode Control Register outputs the PCMIN data from PCMOUT?
If there is an input from MIC, it is added, converted, and output from PCMOUT.
Q2
Is it correct to understand that even if loopback is enabled, the PCMIN audio data will be converted and output from EAR1O (EAR2O)?
-Additional notes below-
Currently, analog input is being input to board A, and analog output is being output from board B via communication.
If you enable board B's loopback from this state, nothing will be output from board B's EAR1OP-N.
Also, when I enabled loopback on board A, which is receiving analog input from MIC1P-N, a waveform similar to the input waveform is output from board A's EAR1OP-N. From these, it appears that the analog side is being looped back rather than the PCM side.
Thanks,
Conor