Randomly fault pin goes low .
1. OUTPUT :BTL mode
a. OUT_A/B : no use
b. OUT_C/D : 4 ohms load
2. INPUT
a. INPUT_A/B : no connection(open)
b. INPUT_C/D : PWM 384KHz
c. INPUT: 20secs volume1 level in and 10secs volume0(mute) level repeat(only 384KHz)---ONLY change
3. GVDD_AB/CD,VDD :+12V (continuously no change)
4. PVDD_AB/CS : +33V (continuously no change)
5. OTW pin no connection(open)
6. randomly fault pin low
If there is anything that could be the cause, please point it out, and if there is something wrong or something that needs to be reviewed, please let me know.