Hi team, I am very new in audio. in the app note slaa894, could you tell me why use 29.5V in step 4?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi team, I am very new in audio. in the app note slaa894, could you tell me why use 29.5V in step 4?
Hello Jingguo,
If you look in the datasheet 29.5V is the highest programmable gain for the amplifier, so this is used to get the Maximum Vout voltage. The Amplifier Gain here represents the "peak voltage" disregarding clipping due to lower PVDD. Measured at 0 dB input(1FS), or a full scale digital input(think the loudest possible signal coming from a digital audio source.)
best regards,
Luis