Part Number: PCM1865
Other Parts Discussed in Thread: PCM1681
Hello, experts.
The data sheet states that the ratio of externally supplied master clocks (SCKI) to the PCM1865 should be 48%~52%.
In addition, the data sheet states that the ratio of externally supplied clocks (SCK) to the PCM1681 should be 40%~60%.
Is it a problem if the clock (SCKI or SCK) deviates significantly from this ratio only about once every 10 seconds?
(PCM1865 is used with SCKI=BCK, and PCM1681 is used with SCK=BCK.)
As long as you listen to the audio in this state, there is no problem.