Part Number: PCM1791A
When using I2C, if you enable external digital filter mode, the PCM1791A sets the MONO bit automatically.
I am guessing this is because the MUTE pin (which would be DATAR when external digital filter mode is enabled) is used as A1 for the I2C interface.
I would have that that A0/A1 were only latched on POR, and the MUTE pin could be used as DATAR after that.
Is this not the case? Do I really have to use SPI in order to be able to use external digital filter mode in stereo?