This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

PCM1820-Q1: PCM1820-Q1

Part Number: PCM1820-Q1
Other Parts Discussed in Thread: PCM1821-Q1

Dears,

I'm serchingh for the best ADC with my target specifations as below 

         -. 2ch analog input upto 2Vrms both Single-ended Line input and differentil Line input

-. Hardware control

-. Master mode 

-. Selection of I2S and TDM output 

-. Best Dynamic range performance ADC

When I serched it in TI website, PCM1820-Q1 is applicable except not Single-ended input 

I'd like check a few things ;

 -. PCM1820-Q1 can't support Single-ended input really?

 -. 7dB degrade Dynamic range in PCM1821-Q1 vs PCM1820-Q1.. Is there no problem if so?

 -.  Is there any device whcih can manage the performance of PCM1820-Q1 and  my requirements?

I will be highly appreciated on your timely feedback 

Thanks

Best regards,

Jaydon