Tool/software:
Hi Team,
Below are the results measured using Audio Precision with the TAS5754M on the PCBA connected directly to the IIS input I/O of the TAS5754.
The test conditions shown in the figure are 26dBV, Po=1W, PVDD=24V, BTL mode
(PS: GAIN is adjusted, but the test result is the same as the picture below, which cannot be consistent with the picture of the Datasheet)
Please tell us how to modify it? (can use hardware or software)
Page 0 0x00 0x01 0x02 0x03 0x04 0x05 0x06 0x07 0x08 0x09 0x0A 0x0B 0x0C 0x0D 0x0E 0x0F ------------------------------------------------------------------------------------------------- 0x00 | 0x00 0x00 0x00 0x00 0x01 0x11 0x00 0x00 0x00 0x00 0x00 0x01 0x7C 0x00 0x00 0x00 0x10 | 0x00 0x00 0x00 0x10 0x00 0x00 0x00 0x00 0x00 0x00 0x80 0x00 0x00 0x00 0x00 0x04 0x20 | 0x00 0x00 0x00 0x01 0x00 0x00 0xF3 0x04 0x02 0x00 0x11 0x01 0x00 0x00 0x00 0x00 0x30 | 0x00 0x00 0x00 0x00 0x00 0x00 0x00 0x00 0x00 0x00 0x00 0x00 0x02 0x30 0x30 0x22 0x40 | 0x02 0x04 0x14 0x05 0x00 0x00 0x00 0x00 0x55 0x00 0x00 0x00 0x00 0x00 0x00 0x00 0x50 | 0x00 0x00 0x00 0x00 0x00 0x00 0x00 0x00 0x81 0x11 0x00 0x36 0x00 0x40 0x00 0x10 0x60 | 0x01 0x10 0x00 0x00 0x00 0x01 0x0F 0x03 0x07 0x10 0xFF 0xD3 0x33 0x00 0x00 0x00 0x70 | 0x80 0x81 0x03 0x00 0x04 0x00 0x85 0x01 0x00 0x00 0x00 0x00 0x00 0x00 0x00 0x00 Page 1 0x00 0x01 0x02 0x03 0x04 0x05 0x06 0x07 0x08 0x09 0x0A 0x0B 0x0C 0x0D 0x0E 0x0F ------------------------------------------------------------------------------------------------- 0x00 | 0x01 0x00 0x00 0x00 0x03 0x00 0x01 0x00 0x00 0x01 0x33 0x11 0x11 0x11 0x00 0x01 0x10 | 0x00 0x00 0x00 0x00 0x00 0x00 0x00 0x00 0x00 0x00 0x00 0x00 0x00 0x00 0x00 0x00 0x20 | 0x00 0x00 0x00 0x00 0x00 0x00 0x00 0x00 0x00 0x00 0x00 0x00 0x00 0x00 0x00 0x00 0x30 | 0x00 0x00 0x00 0x00 0x00 0x00 0x00 0x00 0x00 0x00 0x00 0x00 0x00 0x00 0x00 0x00 0x40 | 0x00 0x00 0x00 0x00 0x00 0x00 0x00 0x00 0x00 0x00 0x00 0x00 0x00 0x00 0x00 0x00 0x50 | 0x00 0x00 0x00 0x00 0x00 0x00 0x00 0x00 0x00 0x00 0x00 0x00 0x00 0x00 0x00 0x00 0x60 | 0x00 0x00 0x00 0x00 0x00 0x00 0x00 0x00 0x00 0x00 0x00 0x00 0x00 0x00 0x00 0x00 0x70 | 0x00 0x00 0x00 0x00 0x00 0x00 0x00 0x00 0x00 0x00 0x00 0x00 0x00 0x00 0x00 0x00 Page 44 0x00 0x01 0x02 0x03 0x04 0x05 0x06 0x07 0x08 0x09 0x0A 0x0B 0x0C 0x0D 0x0E 0x0F ------------------------------------------------------------------------------------------------- 0x00 | 0x2C 0x00 0x00 0x00 0x00 0x00 0x00 0x00 0x00 0x00 0x00 0x00 0x00 0x00 0x00 0x00 0x10 | 0x00 0x00 0x00 0x00 0x00 0x00 0x00 0x00 0x00 0x00 0x00 0x00 0x00 0x00 0x00 0x00 0x20 | 0x00 0x00 0x00 0x00 0x00 0x00 0x00 0x00 0x00 0x00 0x00 0x00 0x00 0x00 0x00 0x00 0x30 | 0x00 0x00 0x00 0x00 0x00 0x00 0x00 0x00 0x00 0x00 0x00 0x00 0x00 0x00 0x00 0x00 0x40 | 0x00 0x00 0x00 0x00 0x00 0x00 0x00 0x00 0x00 0x00 0x00 0x00 0x00 0x00 0x00 0x00 0x50 | 0x00 0x00 0x00 0x00 0x00 0x00 0x00 0x00 0x00 0x00 0x00 0x00 0x00 0x00 0x00 0x00 0x60 | 0x00 0x00 0x00 0x00 0x00 0x00 0x00 0x00 0x00 0x00 0x00 0x00 0x00 0x00 0x00 0x00 0x70 | 0x00 0x00 0x00 0x00 0x00 0x00 0x00 0x00 0x00 0x00 0x00 0x00 0x00 0x00 0x00 0x00 Page 253 0x00 0x01 0x02 0x03 0x04 0x05 0x06 0x07 0x08 0x09 0x0A 0x0B 0x0C 0x0D 0x0E 0x0F ------------------------------------------------------------------------------------------------- 0x00 | 0xFD 0x00 0x00 0x00 0x00 0x00 0x00 0x00 0x00 0x00 0x00 0x00 0x00 0x00 0x00 0x00 0x10 | 0x00 0x00 0x00 0x00 0x00 0x00 0x00 0x00 0x00 0x00 0x00 0x00 0x00 0x00 0x00 0x00 0x20 | 0x00 0x00 0x00 0x00 0x00 0x00 0x00 0x00 0x00 0x00 0x00 0x00 0x00 0x00 0x00 0x00 0x30 | 0x00 0x00 0x00 0x00 0x00 0x00 0x00 0x00 0x00 0x00 0x00 0x00 0x00 0x00 0x00 0x00 0x40 | 0x00 0x00 0x00 0x00 0x00 0x00 0x00 0x00 0x00 0x00 0x00 0x00 0x00 0x00 0x00 0x00 0x50 | 0x00 0x00 0x00 0x00 0x00 0x00 0x00 0x00 0x00 0x00 0x00 0x00 0x00 0x00 0x00 0x00 0x60 | 0x00 0x00 0x00 0x00 0x00 0x00 0x00 0x00 0x00 0x00 0x00 0x00 0x00 0x00 0x00 0x00 0x70 | 0x00 0x00 0x00 0x00 0x00 0x00 0x00 0x00 0x00 0x00 0x00 0x00 0x00 0x00 0x00 0x00