Other Parts Discussed in Thread: TLC555, OPA192
Tool/software:
Hi Team,
As shown in the diagram below, I would like to use two OPA1678 operational amplifiers to drive a piezoelectric buzzer. One of them will serve as an inverting amplifier, while the other will serve as a non-inverting amplifier.
The input voltage in the diagram ranges from DC 5V to 12V, and the analog switch input is a PWM signal from the SOC with a frequency ranging from 1kHz to 4kHz. The two OPA1678 amplifiers will output complementary signals with the same frequency to drive the piezoelectric buzzer.Is this plan feasible?
1、Can OPA1678 be used for square wave signal input? (Frequency 1KHZ~4KHZ).
Thanks