Tool/software:
Could you please help check if the schematic diagram of TAC5112 is correct? If there are any unreasonable aspects, please point them out. Thank you.
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Tool/software:
Could you please help check if the schematic diagram of TAC5112 is correct? If there are any unreasonable aspects, please point them out. Thank you.
Hi Yang,
Schematic looks good, my only comment is that we recommend 1uF coupling caps at the input. You can use 2.2uF, however this will impact the cutoff frequency of the high pass filter created when in an AC coupled configuration. Customer will also have to change charge time in INCAP_QCHG (P0_R5_D[7:6] register.