Other Parts Discussed in Thread: PUREPATHCONSOLE, TAS6424E
Tool/software:
Hi Audio Team,
I am using the TAS6424EQ1EVM for initial evaluation. The evaluation is going well. One of the things I haven't been able to do is prove out the DC Diagnostics. My load is very high > 1K. Reading about the line out impedance it looks like it will be able to handle up to 6kOhm. When I have Line-out enable diagnostics checked I still see an open-load condition when I run the DC Load Diagnostics. In order to play on the high impedance loads I have turned off the DC diagnostics by checking "Bypass LD". Is this the expected behavior? I was hoping to see it would be able to detect the high impedance load. Is there something I should configure differently?
Thanks,
Kessler