Other Parts Discussed in Thread: OPA1652
Tool/software:
Hi,
I designed and built this circuit as a differential ADC input stage.
If I select the x4 gain or x8 gain (changing R3 value) the outputs are completly unbalanced.
If I measure the differential voltage with a multimeter across the two outputs, this is correct.
If I measure the single ended voltage (each output against the ground) the result is unequal, for example with 0.2V input and x8 gain, VF1 is 1.4V and VF2 is -0.2V.
What could be the cause of this behaviour? Maybe this is not the optimal op amp for the application? Something wrong with my circuit ?
thanks