Tool/software:
What is the register address and setting to disable this feature?
I cant find it inside datasheet

This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi Joo,
This is controlled by Book 0 Page 0 Register 0x3e Bit 4:
Best regards,
-Ivan Salazar
Applications Engineer
Hi Ivan;
JY is also asking:
What is the default register setting value and can I have details of each bit for 0x3E? Any other register else will control the idle channel detect?
Hi Joo, David,
Yes, Idle Channel Detect feature is enabled by default.
Default value of register 0x03e is 0x10. Only this register should control the feature.
Best regards,
-Ivan Salazar
Applications Engineer
Hi Ivan,
I tried to use purepath try to change the Idle Channel Detection threshold.
But after change, i didnt see any change in the register setting map.
What is the register address to change the threshold?
Beside that, what is the default threshold for Idle Channel Detection?
Hi Joo,
Did you use the "apply" button at the top-right after changing the threshold?
It is still recommended to use PPC3 to generate the proper coefficient values, as it will account for any value range limitations.
Best regards,
-Ivan Salazar
Applications Engineer