This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TLV320AIC3111: how to generate ADC Biquad Filter Coefficients and ADC Biquad Filter Coefficients

Part Number: TLV320AIC3111TLV320AIC3110
Other Parts Discussed in Thread: TLV320AIC3111, TLV320AIC3110

Tool/software:

Hi 

I use TLV320AIC3111/TLV320AIC3110 for my design, but I can't find how to generate ADC/DAC Biquad Filter Coefficients and ADC/DAC FIR Filter Coefficients,

meanwhile I don't find any details about 3D PGA(how to enable and adjust).

Can you share more information with me?

  • Hi Zhou,

    The TI Biquad tool will allow you to determine the proper coefficients. https://www.ti.com/tool/COEFFICIENT-CALC Set your sample rate and then create your biquad frequency response that you want. Then click the "coefficient" button to see the proper coefficients to load into the device.

    I have reached out to our design team on clarification on the 3D PGA.

    Best regards,
    Jeff McPherson

  • Hi :

    Thank you for your reply.

    What about ADC/DAC FIR Filter Coefficients?

    can you help confirm too?

  • Hi Zhou,

    The biquad tool includes the filters for the FIR. These are 1st order filters and so in the biquad tool they are listed as "1O" 

    You will see the transfer function for the FIR filter matches that of the 1O filter in the BQ tool.

    Best regards,
    Jeff McPherson

  • Hi :

    Thank you for your reply.

    Is there any update about 3D PGA?

  • Hi Zhou,

    I did not hear back but I found something that may help.

    From what I can gather the 3D PGA coefficient is a measure of how intense the 3D effect is:

    A value of 0 means the effect is off, a normal stereo mix.
    A maximum value 0x7FFFF means that the effect is turned all the way on, creating a wide stereo image.
    A minimum value of 0xFFFFF means that the Left and Right channels have been swapped. 

    You can think of it as this: the more positive the coefficient, the wider the channels become. The more negative the coefficient, the closer together the channels become, first becoming a mono mix, and then swapping L and R completely. 

    The EVM control software for the AIC3254 has a GUI for this.

    You can drag the slider to the left or right based on how intense the effect you want. The value in the lower right is the decimal value of the coefficient required. If you convert this to hex, you can write this to the AIC3111. Because the AIC3111 and the AIC3254 have similar processing blocks, I am confident this GUI will get you the correct values.

    Best regards,
    Jeff McPherson

  • Hi :

    As showing in datasheet, I think 3111 is different from 3254.

    First, the maximum value should be 7FFF while minimum value should be 8000.

    Then the parameters can't switch dynamatically, it need set to page 12 first then switch to page 12. 

    So I think it should be something like this:

    w 30 00 0C
    w 30 40 7F FF

    w 30 00 08
    w 30 01 05

    But when I send command as above, the page 8 / register 1, bit D0 doesn't set back to 0, it will always be 1, and  page 8 / register 1, bit D1 is 0 too.

    Is there anything wrong?

  • Hi Zhou,

    Thank you for the correction. Are you providing I2S clocks to the device? The buffer swap won't happen unless I2S is provided.

    Also the buffer swapping should be enabled before attempting to write to the coefficients if you're going to use it. 

    Best regards,
    Jeff McPherson

  • Hi :

    >Are you providing I2S clocks to the device? 

    ---->I think yes, because I send command during playing music.

    >Also the buffer swapping should be enabled before attempting to write to the coefficients if you're going to use it. 

    ---->Do you mean I should send command as follows? I tried but the result is same, the page 8 / register 1, bit D0 doesn't set back to 0, it will always be 1, and  page 8 / register 1, bit D1 is 0 too.

    w 30 00 08
    w 30 01 05

    w 30 00 0C
    w 30 40 7F FF

  • Hi Zhou,

    Sorry I was not clear. I meant that the buffer swapping should be enabled before the DAC is powered on. As the data sheet mentions, while the DAC is running the coefficients are locked. If the DAC is powered on before the buffer swapping is enabled, then the turning the swapping on after the DAC is running will not work.

    Best regards,
    Jeff McPherson

  • Hi :

    If so, what does this line(whith red box) mean?

    I think buffer swapping is added for swap coefficients during DAC is running.

  • Hi Zhou,

    In the paragraph above, the double buffering is turned on through page 8 register 1 bit 2. Once the double buffering is enabled, then you can swap the buffers using page 8 register 1 bit 0. It looks like your code is trying to swap the buffers before enabling the feature.

    Best regards,
    Jeff McPherson

  • Hi :

    the data of register 01 page 8 is 0x04 before I run command below, so I think it is correct.

    the reason why "the page 8 / register 1, bit D0 doesn't set back to 0, it will always be 1, and  page 8 / register 1, bit D1 is 0 too" is the control software doesn't read data from AIC3111 when I click refresh, after I read manully, it is correct, so I close this question:

    w 30 00 0C
    w 30 40 7F FF

    w 30 00 08

    w 30 01 05