Other Parts Discussed in Thread: TAS2572, TAS2563
Tool/software:
I have been wrestling with a simple dilemma that has turned out to be more complex that I thought. I am designing a micro amplifier that I want to be able to make 5 watts per channel but supplied with a single cell lithium ion battery.
So minimum voltage would be 3 and max would be 4.2v. The battery is a high current draw and I want very high quality audio so a DC to DC converter to increase the voltage to the amplifier seems like it would add too much noise to the DC current.
Does the TAS2764 which is rated for the voltage, give high enough wattage at 3 volts supply into a 4 ohms speaker and able to get 4 or 5 watts?
Am I also barking up the wrong tree with this design. The PCB board is roughly 10cm² and I am using a 18650 battery.