Tool/software:
Hello,
We have bouhgt the TLV320AIC3254 EVM
and we are currently in the middle of the design the TLV320AIC3254 component
i would like to ask for a schematic review (Attached PDF also)
also i have few questions
1. 1.8V and 3.3V are externally powered (on another page)
2. I2C and I2S(WCLK,BCLK,DIN,DOUT) and etc... are connected to FPGA (on another page)
and a few questions:
1.How can i implemnt MONO sound? ( input and High power output)
do i need to short between L and R? or do i connect only R ?
2.how do i implement the headset detect?
3.what is the diffrence between Line Output and High power Output?
can i use only High power output?
4. How do i implement or connect here Volume Up/Down
Thank You,
Amit Perry