Other Parts Discussed in Thread: OPA1622, , TINA-TI, BUF634, BUF634A, OPA1633
Tool/software:
Hi,
I am designing a headphone amplifier for use in recording studio applications. It will need to drive high-impedance headphones to loud studio volumes.
I'm using the AK4499EX current-mode DAC. I have based a headphone amp design on the reference TI design https://www.ti.com/lit/ug/tidu672c/tidu672c.pdf?ts=1723909825481. The product is powered by a 12V supply which I'm regulating down to ±10V rails, and I'd like the output to swing as close to these rails as possible.
I modified the design to match the DAC; the transimpedance stage swings to ±9.1V and the OPA1622 has 0.5x gain to give a single-ended ±9.1V output. I would like more current than a single OPA1622 can provide so I have inserted an LME49600.
I am facing a simulation issue. The circuit behaves as designed if VCC / VEE are changed to 17V or greater. However, I'd like this circuit to operate on a lower voltage, ideally ±10V supply rails which can be cleanly derived from an unregulated 12V supply.
Could someone explain this behaviour? At ±16V the circuit should behave correctly but TINA-TI fails to run a transient simulation.
I would appreciate any suggestions or comments for a better headphone amplifier design. Is there a part like the LME49600 which will swing closer to the output rails? Could I instead parallel a second OPA1622? Or should I redesign the product with ±15V rails?
Attached a TINA-TI screenshot and a file. Running "Transient Analysis" it will fail, changing VCC and VEE to 17V will make the simulation work.
Max