This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

OPA1622: studio headphone amplifier design review

Part Number: OPA1622

Tool/software:

Hi,

I am making a studio headphone amplifier product based on the AK4499EX DAC (as discussed in a linked post). I would like more output power than a single OPA1622 can provide (300mA current would be ideal, even at hot temperatures). I have come up with the following design. I would love any feedback!

Schematic PDF and TINA file/screenshot attached.

XEBRA-A3.TSC

DAC.pdf

  • Hi Max, 

    I checked over your design in Tina. It appears to work fine and makes sense. If you are concerned at all about any spikes on the output due to plugging in and unplugging cables you may consider using TVS protection diodes on the board. This could even just be footprints for TVS protection in the event you find you need them. 

    TVS Diodes:

    https://www.ti.com/interface/diodes/tvs-diodes/overview.html

    One thing to note with the ballast resistors on the outputs is that there will be some associated offset voltage between amps and therefore not all the expected current will reach the load. Instead of 300 mA you may see somewhat less. The offset voltage between the amps will show up at the outputs of each and some current will be going into the some output(s). This may be insignificant for your design however. You will still see a significant increase in output drive capability with your method however. 

    An alternative idea is shown below 

    https://www.ti.com/lit/ab/sboa352/sboa352.pdf?ts=1724197923030&ref_url=https%253A%252F%252Fwww.ti.com%252Fproduct%252FINA1620

    All in all I think your design looks good!

    Best Regards, 

    Chris Featherstone

  • Thanks Chris! With the maximum DC offset of 0.5mV I should be losing at most 1mA right?

    Where should I put the TVS diodes? If you look at the attached PDF the headphone amplifier is connected directly to a DAC. I'm not sure where/how the TVS would help?