Tool/software:
Hi
Customer have some issue need some advice
1. If the input exceeds 50%, it will produce a popping sound
2. The filtering capacitor at the power supply point will pull down the supply voltage, causing other voltages in the system to also be pulled down. After removing it, it is OK. When using a voltage regulator to supply power to the amplifier alone, the filtering capacitor will not affect the supply voltage.
The SCH as attachment.