The TI E2E™ design support forums will undergo maintenance from July 11 to July 13. If you need design support during this time, open a new support request with our customer support center.

This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

PCM1681: Output of clipped SINE waveforms

Part Number: PCM1681

Tool/software:

Hello, experts.

Please tell me about the output of the clipped SINE waveform of the PCM1681 as soon as possible.

The figure below shows the circuit configuration and the observation waveform when the clipped SINE waveform is output from the FPGA.

At 1 kHz and 2 kHz, the waveform is output normally, but at 3 kHz, the waveform is not output properly.(Red arrows)

The output data from the FPGA to the DAC is shown in the figure below.

The PCM1681 is the H/W control, LRCK = 16kHz, MCLK = BICK = 4.096MHz (=256fs).

The LPF circuit is shown in the figure below.

Please tell me how to output the clipped 3kHz (the same as the output of the FPGA) from the PCM1681.

Best regards.

Kiyama

  • Hello Kiyama,

    Please disconnect the load and have a simple LPF first and verify the problem is still there and it is not coming from the loading of your active filter.

    Another test that I need you to do next,  is  to directly send a -1dBFS sinewave to the DAC and monitor the outcome( with your filter still removed and simple LPF in place)

    Would you please confirm the channel depth and number of channels you are using. 

    If using HW or SW control what is FMT0/1 values?

    Regards,

    Arash