This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPA3128D2: Absolute Maximum Ratings

Part Number: TPA3128D2

Tool/software:

Datasheet shows the input voltage rage -0.3 to 6.3V on "INPL","INNL", "INPR","INNR".

Is this meaning "DC cut signal should be less than 0.6Vp-p"? More higher level signal exceed negative limit of 0.3V.

If I wish to input signals as 6Vp-p, then should aI need bias as 3.0V to hold the signnal within 6.3V?

This (or ather) amp works with the limit of supply voltage, and such higher signal ccaa not be amplified due to the limit of supply, however the previous stage might output such higher level signal, then I would like to know it makes damaged on this amp.