This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TLV320AIC3104: Application issues of chips

Part Number: TLV320AIC3104


Tool/software:

After powering on, there is sound coming from the MIC string to the speaker and the loopback is not turned on. The audio playback is normal. Can you help me identify the hardware and software issues and how to solve them? For example, which register setting is related to this?
In addition, QIIC is used to read the value of the codec register. AT+QIIC=<1>,<2>,<3>The third parameter is the register address, which reads its value

[2024-09-04_18:08:22:241]AT+QIIC=1,0x18,0,1

[2024-09-04_18:08:22:397]+QIIC: 0x00

[2024-09-04_18:08:22:397]OK
[2024-09-04_18:08:22:427]AT+QIIC=1,0x18,3,1

[2024-09-04_18:08:22:549]+QIIC: 0x10

[2024-09-04_18:08:22:549]OK
[2024-09-04_18:08:22:610]AT+QIIC=1,0x18,6,1

[2024-09-04_18:08:22:685]+QIIC: 0x00

[2024-09-04_18:08:22:685]OK
[2024-09-04_18:08:22:731]AT+QIIC=1,0x18,8,1

[2024-09-04_18:08:22:807]+QIIC: 0x00

[2024-09-04_18:08:22:807]OK
[2024-09-04_18:08:22:822]AT+QIIC=1,0x18,10,1

[2024-09-04_18:08:22:977]+QIIC: 0x00

[2024-09-04_18:08:22:977]OK
[2024-09-04_18:08:23:008]AT+QIIC=1,0x18,16,1

[2024-09-04_18:08:23:116]+QIIC: 0x80

[2024-09-04_18:08:23:116]OK
[2024-09-04_18:08:23:132]AT+QIIC=1,0x18,20,1

[2024-09-04_18:08:23:283]+QIIC: 0x78

[2024-09-04_18:08:23:283]OK
[2024-09-04_18:08:23:375]AT+QIIC=1,0x18,26,1

[2024-09-04_18:08:23:375]+QIIC: 0x00

[2024-09-04_18:08:23:375]OK
[2024-09-04_18:09:43:343]AT+QIIC=1,0x18,29,1

[2024-09-04_18:09:43:369]+QIIC: 0x00

[2024-09-04_18:09:43:369]OK
[2024-09-04_18:09:43:391]AT+QIIC=1,0x18,30,1

[2024-09-04_18:09:43:416]+QIIC: 0xfe

[2024-09-04_18:09:43:416]OK
[2024-09-04_18:09:43:443]AT+QIIC=1,0x18,31,1

[2024-09-04_18:09:43:467]+QIIC: 0x00

[2024-09-04_18:09:43:467]OK
[2024-09-04_18:09:43:494]AT+QIIC=1,0x18,32,1

[2024-09-04_18:09:43:524]+QIIC: 0x80

[2024-09-04_18:09:43:524]OK
[2024-09-04_18:09:43:544]AT+QIIC=1,0x18,33,1

[2024-09-04_18:09:43:569]+QIIC: 0x01

[2024-09-04_18:09:43:569]OK
[2024-09-04_18:09:43:596]AT+QIIC=1,0x18,34,1

[2024-09-04_18:09:43:625]+QIIC: 0x00

[2024-09-04_18:09:43:625]OK
[2024-09-04_18:09:43:645]AT+QIIC=1,0x18,35,1

[2024-09-04_18:09:43:668]+QIIC: 0x00

[2024-09-04_18:09:43:668]OK
[2024-09-04_18:09:43:698]AT+QIIC=1,0x18,36,1

[2024-09-04_18:09:43:724]+QIIC: 0x00

[2024-09-04_18:09:43:724]OK
[2024-09-04_18:09:43:748]AT+QIIC=1,0x18,37,1

[2024-09-04_18:09:43:771]+QIIC: 0x00

[2024-09-04_18:09:43:771]OK
[2024-09-04_18:09:43:798]AT+QIIC=1,0x18,38,1

[2024-09-04_18:09:43:827]+QIIC: 0x00

[2024-09-04_18:09:43:827]OK
[2024-09-04_18:09:43:838]AT+QIIC=1,0x18,40,1

[2024-09-04_18:09:43:863]+QIIC: 0x00

[2024-09-04_18:09:43:863]OK
[2024-09-04_18:09:43:879]AT+QIIC=1,0x18,42,1

[2024-09-04_18:09:43:907]+QIIC: 0x00

[2024-09-04_18:09:43:907]OK
[2024-09-04_18:09:43:921]AT+QIIC=1,0x18,44,1

[2024-09-04_18:09:43:947]+QIIC: 0x80

[2024-09-04_18:09:43:947]OK
[2024-09-04_18:09:43:962]AT+QIIC=1,0x18,46,1

[2024-09-04_18:09:43:991]+QIIC: 0x00

[2024-09-04_18:09:43:991]OK
[2024-09-04_18:09:44:004]AT+QIIC=1,0x18,48,1

[2024-09-04_18:09:44:027]+QIIC: 0x00

[2024-09-04_18:09:44:027]OK
[2024-09-04_18:09:44:044]AT+QIIC=1,0x18,50,1

[2024-09-04_18:09:44:070]+QIIC: 0x00

[2024-09-04_18:09:44:070]OK
[2024-09-04_18:09:44:084]AT+QIIC=1,0x18,52,1

[2024-09-04_18:09:44:109]+QIIC: 0x00

[2024-09-04_18:09:44:109]OK
[2024-09-04_18:09:44:125]AT+QIIC=1,0x18,54,1

[2024-09-04_18:09:44:154]+QIIC: 0x00

[2024-09-04_18:09:44:154]OK
[2024-09-04_18:09:44:166]AT+QIIC=1,0x18,56,1

[2024-09-04_18:09:44:194]+QIIC: 0x00

[2024-09-04_18:09:44:194]OK
[2024-09-04_18:10:59:251]AT+QIIC=1,0x18,58,1

[2024-09-04_18:10:59:276]+QIIC: 0x04

[2024-09-04_18:10:59:276]OK
[2024-09-04_18:10:59:299]AT+QIIC=1,0x18,59,1

[2024-09-04_18:10:59:322]+QIIC: 0x00

[2024-09-04_18:10:59:322]OK
[2024-09-04_18:10:59:354]AT+QIIC=1,0x18,60,1

[2024-09-04_18:10:59:378]+QIIC: 0x00

[2024-09-04_18:10:59:378]OK
[2024-09-04_18:10:59:402]AT+QIIC=1,0x18,61,1

[2024-09-04_18:10:59:425]+QIIC: 0x00

[2024-09-04_18:10:59:425]OK
[2024-09-04_18:10:59:451]AT+QIIC=1,0x18,62,1

[2024-09-04_18:10:59:475]+QIIC: 0x00

[2024-09-04_18:10:59:475]OK
[2024-09-04_18:10:59:505]AT+QIIC=1,0x18,63,1

[2024-09-04_18:10:59:529]+QIIC: 0x00

[2024-09-04_18:10:59:529]OK
[2024-09-04_18:10:59:555]AT+QIIC=1,0x18,64,1

[2024-09-04_18:10:59:588]+QIIC: 0x00

[2024-09-04_18:10:59:588]OK
[2024-09-04_18:10:59:603]AT+QIIC=1,0x18,65,1

[2024-09-04_18:10:59:627]+QIIC: 0x04

[2024-09-04_18:10:59:627]OK
[2024-09-04_18:10:59:654]AT+QIIC=1,0x18,66,1

[2024-09-04_18:10:59:679]+QIIC: 0x00

[2024-09-04_18:10:59:679]OK
[2024-09-04_18:10:59:708]AT+QIIC=1,0x18,67,1

[2024-09-04_18:10:59:728]+QIIC: 0x00

[2024-09-04_18:10:59:728]OK
[2024-09-04_18:10:59:748]AT+QIIC=1,0x18,69,1

[2024-09-04_18:10:59:768]+QIIC: 0x00

[2024-09-04_18:10:59:768]OK
[2024-09-04_18:10:59:788]AT+QIIC=1,0x18,71,1

[2024-09-04_18:10:59:810]+QIIC: 0x00

[2024-09-04_18:10:59:810]OK
[2024-09-04_18:10:59:830]AT+QIIC=1,0x18,73,1

[2024-09-04_18:10:59:854]+QIIC: 0x00

[2024-09-04_18:10:59:854]OK
[2024-09-04_18:10:59:871]AT+QIIC=1,0x18,75,1

[2024-09-04_18:10:59:895]+QIIC: 0x00

[2024-09-04_18:10:59:895]OK
[2024-09-04_18:10:59:912]AT+QIIC=1,0x18,77,1

[2024-09-04_18:10:59:944]+QIIC: 0x00

[2024-09-04_18:10:59:944]OK
[2024-09-04_18:10:59:952]AT+QIIC=1,0x18,79,1

[2024-09-04_18:10:59:974]+QIIC: 0x00

[2024-09-04_18:10:59:974]OK
[2024-09-04_18:10:59:993]AT+QIIC=1,0x18,81,1

[2024-09-04_18:11:00:017]+QIIC: 0x00

[2024-09-04_18:11:00:017]OK
[2024-09-04_18:11:00:036]AT+QIIC=1,0x18,83,1

[2024-09-04_18:11:00:059]+QIIC: 0x00

[2024-09-04_18:11:00:059]OK
[2024-09-04_18:11:00:074]AT+QIIC=1,0x18,85,1

[2024-09-04_18:11:00:106]+QIIC: 0x00

[2024-09-04_18:11:00:106]OK
[2024-09-04_18:11:42:481]AT+QIIC=1,0x18,87,1

[2024-09-04_18:11:42:517]+QIIC: 0x00

[2024-09-04_18:11:42:517]OK
[2024-09-04_18:11:42:527]AT+QIIC=1,0x18,88,1

[2024-09-04_18:11:42:548]+QIIC: 0x00

[2024-09-04_18:11:42:548]OK
[2024-09-04_18:11:42:578]AT+QIIC=1,0x18,89,1

[2024-09-04_18:11:42:601]+QIIC: 0x00

[2024-09-04_18:11:42:601]OK
[2024-09-04_18:11:42:630]AT+QIIC=1,0x18,90,1

[2024-09-04_18:11:42:660]+QIIC: 0x00

[2024-09-04_18:11:42:660]OK
[2024-09-04_18:11:42:680]AT+QIIC=1,0x18,91,1

[2024-09-04_18:11:42:703]+QIIC: 0x00

[2024-09-04_18:11:42:703]OK
[2024-09-04_18:11:42:733]AT+QIIC=1,0x18,92,1

[2024-09-04_18:11:42:758]+QIIC: 0x00

[2024-09-04_18:11:42:758]OK
[2024-09-04_18:11:42:781]AT+QIIC=1,0x18,93,1

[2024-09-04_18:11:42:805]+QIIC: 0x00

[2024-09-04_18:11:42:805]OK
[2024-09-04_18:11:42:833]AT+QIIC=1,0x18,94,1

[2024-09-04_18:11:42:855]+QIIC: 0x00

[2024-09-04_18:11:42:855]OK
[2024-09-04_18:11:42:883]AT+QIIC=1,0x18,95,1

[2024-09-04_18:11:42:906]+QIIC: 0x00

[2024-09-04_18:11:42:906]OK
[2024-09-04_18:11:42:937]AT+QIIC=1,0x18,96,1

[2024-09-04_18:11:42:957]+QIIC: 0x00

[2024-09-04_18:11:42:957]OK
[2024-09-04_18:11:42:972]AT+QIIC=1,0x18,98,1

[2024-09-04_18:11:42:998]+QIIC: 0x00

[2024-09-04_18:11:42:998]OK
[2024-09-04_18:11:43:017]AT+QIIC=1,0x18,100,1

[2024-09-04_18:11:43:037]+QIIC: 0x00

[2024-09-04_18:11:43:037]OK
[2024-09-04_18:11:43:057]AT+QIIC=1,0x18,102,1

[2024-09-04_18:11:43:078]+QIIC: 0x02

[2024-09-04_18:11:43:078]OK