Tool/software:
About TLV320AIC3110
I would like to connect this IC to Linux and use it by connecting a microphone and speaker.
At this time, two unintended symptoms (1) and (2) appear, so I would like to resolve them.
What are the possible causes?
(1) Recording will end in 1/3 of the set time. When played back on Linux, the sound is as recorded, but on a PC it plays at 1/3 speed, giving the impression of a lag.
(2)Sound pressure becomes extremely low.
When I play
Pattern A :repeatedly with "aplay" command, the sound pressure drops at some point and then stays low until I restart the computer(reset IC).
Pattern B: Sound pressure is low from the time of startup.
Thanks.