Part Number: PCMD3140
Tool/software:
Hi,
If I use only 2 channels, do I need to NC process PDMDIN2_GPI2 pins?

This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi,
If you are using only two digital mic channels, the two mics can be connected to GPI1 as shown in the above diagram.
Since the GPI2 pin is an input pin, we can connect it to GND (we can also disable the GPI2 pin function through the GPI2_CFG[2:0] bit fields).

Thanks and Regards,
Lakshmi Narasimhan