This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LCFILTER-CALC-TOOL: LC filter

Part Number: LCFILTER-CALC-TOOL

Tool/software:

Please suggest an filter for following spec.

Type

Low Pass

Filter Order

3rd

Technology

LC (T-Type)

Technology

LC (T-Type)

Number of Channels

1

Center / Cutoff Frequency

135MHz (Cutoff)

Attenuation Value

25dB @ 300MHz ~ 450MHz

Resistance - Channel (Ohms)

0.05

Current

2:00 AM

Values

C = 100pF

ESD Protection

No

Operating Temperature

-40°C ~ 85°C

Applications

Data Lines for Mobile Devices

Voltage - Rated

50V

Mounting Type

Surface Mount

 

Regards,

Nishalini Baskaran

  • Hi Nishalini,

    Your post got assigned to audio support team, but this does not seem like it. Is there a TI device you're using in which the LCL filter is required? Please use the TI device part number whenever creating a new post, this helps to assign your question to the proper support team.

    Best regards,
    -Ivan Salazar
    Applications Engineer