Part Number: TAS2505EVM
Other Parts Discussed in Thread: TAS2505-Q1, TAS2505
Tool/software:
==≈======================
My specifications and register settings
OutDAC: Class D
Input : TDM or I2S
Speaker load: 8Ω/2W
SPKVDD: 5V
MCLK frequency: Undetermined
Reg63 ”DAC Channel Volume Control's Soft-Step control”...Soft-Stepping is 1 step per 1 or 2 DAC Word Clock
==========================
I would like to check whether there is any pop noise when switching from maximum volume to MUTE with a Class D amplifier. Are there any experimental videos or test data using an evaluation board?
*It does not have to be an evaluation board, as long as you have test data for the TAS2505 or TAS2505-Q1
P.S. ====
Please also answer the following questions. ↓
Is it possible to completely eliminate the pop noise by adjusting the soft-stepping change rate (DAC fs, Reg63)?
If this is not possible, is it possible to eliminate the noise when muted using an external circuit?