Part Number: TPA6304-Q1
Tool/software:
There is a derivative model of 26SA that needs to add SUBWOOFER. We use TPA6304 as the amplifier of SUBWOOFER. SUBWOOFER speaker only needs one Channel. The circuit is as the attachment:TPA6304-Q1.pdf
IC1200 for 4CH amp.
IC1205 for 1CH subwoofer amp.
My question as below
1.For 4CH amp, we need to change the input capacitor(C1236/C1240/C1241/C1242) from 0.47uF to 0.33uF for the audio quality improvement. So can the IN_REF capacitance change from 2.2uF to 1uF?
Does the input capacitor capacitance for 1CH to the IN_REF capacitor capacitance need 1:4 ?
2.For 1CH subwoofer amp, we only use one Channel , If the input capacitor (C1255) capacitance to be 0.33uF, what is the capacitance of the C1388? 0.33uF ?
3.For 1CH subwoofer amp, There are three channels not used , their output load is open. So the FAULT pin will send out the low level to our SOC for DC diagnostics.
How can we disable the three unused pin DC diagnostics?
Thanks!