Part Number: TPA6304-Q1
Tool/software:
Hi team,
I have a few questions about the spread spectrum of 6304 that I would like to confirm. The specification states that the following registers need to be modified for LOW EMI.

1) SSC1: Both Low EMI and reset are written as 0x22, but in the description in the red box, after reset it is 0x82. If I want to enable Low EMI mode, do I need to write 0x82 here or just keep the default?

2) SSC2: Why is only SSC2 turned off in Low EMI mode? If you want to turn on SSC2 and SSC3 at the same time, is 0x80→0xA2 correct?

3) I want to confirm what is the variable frequency range of the SSC spread spectrum of 6304? Is there a register to set it?